Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
IGBT and SLLIMM IPM Slide 26

Please note that the addition of the STGIPN3H60A and STGIPN3H60-H are new devices that round out our existing two offerings by offering devices with the Hin and Lin input logic as all Active High as requested by some customers to meet their MCU requirements. The STGIPMN3H60AT and STGIPN3H60T-H will also add the desired NTC thermistor feature for temperature sensing on the module. A proposed 5 A, 600 V device not shown on this table is up to a year from being available.

PTM Veröffentlicht am: