Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
IGBT and SLLIMM IPM Slide 33

The SLLIMM Gen 2 package positioning is shown on this slide, with end product applications on the vertical axis and power on the horizontal axis. The FM package targets lower power applications due to its lesser capability of removing heat from the IGBTs, as the heat must be conducted away from the devices through the epoxy package. It has lower thermal conductivity than the more effective Direct Bonded Copper package. The DBC package targets higher power and performance applications that can support its higher cost.

PTM Veröffentlicht am: