Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 8

The image shown here shows the critical components that exist within each RF reed relay. One can see the double shield connections on each side of the relay. The four shield points and the two signal leads make up the key components of the RF relay. The two coil leads turn the relay on and off, opening and closing the reed switch contacts, but play no role in the RF characteristics.

PTM Veröffentlicht am: