Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 6

The impedance can be calculated at any point along the signal path. In this manner the designer will know ahead of time if one is meeting the 50 Ω. Therefore the RF signals look at the distributed impedance along the signal path. So when the RF comes upon a change in impedance (say 55 Ω instead of 50 Ω), part of the signal where the impedance has changed will be reflected backwards. This translates into an actual loss in signal strength.

PTM Veröffentlicht am: