Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 13

Shown here are the geometric dimensions with the leads after they have exited molded plastic. At this point, the shield and signal leads encounter a ground plane where the leads are mounted on a substrate. Since this is also a standard lead configuration with ground plane, there are standard programs available to simply add the dimensions to the program which will, in turn, output the exact characteristic impedance.

PTM Veröffentlicht am: