Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
RF Reed Relays Presentation - Part 2 Slide 20

Shortening the signal path will improve the RF characteristics of the reed relay. Standex Electronics’ LP Series was one of the first RF relays. With new relay designs Standex Electronics has dramatically reduced the overall signal path. The signal path starts at the bottom of the PCB at point A, goes thru the PCB, up into the junction of the reed switch, thru the reed switch and down to the bottom of the PCB. The distance within the relay from point A to B is approximately 0.8 inches with the added length from the bottom of the PCB on both sides and up into the relay. This offers much room for improvement as will be shown next.

PTM Veröffentlicht am: