Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide6

The hermetically sealed reed sensors are ideal under harsh environmental conditions that typically exist in under-the-hood environments. Here the dirty, corrosive, expansive temperature range has no negative effect on the reed sensor’s operating characteristics. Reed sensors, unlike mechanical sensors offer remote sensing at distances greater than one inch. Of course, non-ferromagnetic metals and plastics offer no interference to their magnetic sensitivity. This allows the reed sensor to be placed in a benign environment out of harm’s way. Reed sensors do not require any power when they are in their off or un-energized state making them ideal for battery operated applications. This is not the case with solid state sensors that use power 100% of the time.

PTM Veröffentlicht am: