Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide32

The reed sensor’s wide operating temperature ensures reliable operation at extreme temperatures. This is not the case with some solid state sensors that not only require power 100% of the time, but also are derated at higher temperatures. The reed sensor does not draw any power until energized. Also, reed sensors have the ability to switch billions of consistent fault-free operations over their lifetime. To ensure fault-free operation, Standex Electronics tests each sensor dynamically for thousands of operations on every reed sensor that is sent to the customer. This dynamic contact resistance test has the ability to detect potential early failures which are eliminated from shipment.

PTM Veröffentlicht am: