Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide14

Almost all the automotive manufacturers in the world have selected some form of reed sensor for monitoring the brake fluid level. The reed switch by itself is hermetically sealed, which guards against the effects of dirty harsh environments. Because of these harsh environments and extreme temperature swings, some suppliers provide the reed sensor in a vapor sealed plastic package for further insurance of proper operation in ‘under the hood’ conditions. Reed sensors have the ability to operate for billions of fault free operations. To ensure fault free operation, Standex Electronics tests each sensor dynamically for thousands of operations on every reed sensor that is sent to the customer. This dynamic contact resistance test has the ability to detect potential early failures which are eliminated from shipment.

PTM Veröffentlicht am: