Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide30

The reed switch is hermetically sealed. Electromechanical and semiconductor sensors are not hermetically sealed. In many of the window washer sensing requirements, manufacturers are choosing a turnkey reed sensor. This means that the reed sensor incorporates a sensing float that rides with the rise and fall of the liquid. It has an embedded magnet that will activate the reed sensor once the float comes within sensing distance of the hermetically sealed reed switch. The reed switch will in turn activate an indicator light and also supply a signal to the on-board computer. The hermetically sealed reed switch can also switch power as well as very low level digital signals directly. Electromechanical and solid state sensing technologies cannot carry out both functions directly. They will need additional components, which add more cost.

PTM Veröffentlicht am: