Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide31

To better understand the benefit of the Cellular Framework, the designer will take a moment to discuss what development looks like without a framework. First, there is the physical components. This is the same regardless. When the designer integrates the cellular modem support, which usually requires integration from the low level modem interface all the way up to the application code layer, the modem support affects all layers, meaning any change could potentially impact other parts of the code that the designer may not be aware of. It also tends to be fairly large and is invasive, causing the developer to spend more time integrating and debugging. When creating cellular applications, developers often face the issue of using one cellular modem for evaluation and having to start over with another modem for production.

PTM Veröffentlicht am: