Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide3

If asked to describe the ideal connectivity solution for Internet of Things applications, most developers would come to a consensus around the following: First, they would describe a solution that has a long range, as this would enable a device to be placed and go anywhere. Many IoT application designs require sensors to be placed in more locations in order for the state of everything to be known. Some of these locations do not have easy access to a power source, and so, as anyone who has changed a smoke alarm battery in the middle of the night can tell, long battery life matters. So, developers would also say that it’s crucial for a device to have a long battery life. Lastly, as with many technologies, while the solution may exist, the cost of the solution can put it out of reach for most IoT embedded devices. Therefore, a connectivity solution that is also low cost would be high on the developers list of ideal elements.

PTM Veröffentlicht am: