Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide20

For Cellular, the AE-CLOUD2 also comes with cellular and GPS antennas that are attached as they are pictured on this slide. The antennas provide a balance between antenna size and improved cellular and GPS reception. AE-CLOUD2 is powered via the micro USB port shown in the picture. The micro USB port can be connected to a computer USB port, USB wall plug, or even a USB battery power bank for increased portability.

PTM Veröffentlicht am: