Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
AECLOUD-Slide26

Developers can begin to use the cellular connectivity for AE-CLOUD2 using the Cloud Toolbox Demo by following the steps listed. First, the Cloud Toolbox demo code should be loaded onto the AE-CLOUD2 board following the instructions listed in the "Cloud Toolbox Demo Quick Start Guide for the AE-CLOUD2". After the code is loaded, users will configure the cellular carrier settings for the SIM card they have acquired using the command line interface. Users can select from a list of mobile carriers where the settings have been pre-configured in the Cloud Toolbox Demo. If the user has a SIM card from a mobile carrier not on the list, the Cloud Toolbox Demo has a manual mode that allows users to manually connect to the network for a mobile carrier using the AT command set. Next, the user should setup their credentials so that their AE-CLOUD2 kit can connect to the Cloud Toolbox Dashboard where they can visualize and see their sensor data. After the cellular carrier settings have been configured for the AE-CLOUD2, the Cloud Toolbox Demo code will automatically connect to the configured cellular carrier. The user does not need to use the command line interface except for making changes to the current configuration.

PTM Veröffentlicht am: