Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
ELUM-Slide8

The ELUM™ is a single-pole double-throw contact (SPDT) switch that allows normally-closed and normally-open configurations. The ELUM is a make-before-break or shorting switch. The ELUM can also be configured for SPST use. For normally open SPST functions, only terminals 3 and 2 are used. For normally closed SPST functions, only terminals 3 & 4 are used.

PTM Veröffentlicht am: