Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
ELUM-Slide7

The ELUM™ is also able to function as either a signal or a power switch.  It is compatible with signals as low as 10µA at 20mV DC, or with power signals up to 0.25A at 50V DC. In addition to this, the dielectric strength is greater than 250Vrms and the contact resistance is less than 50mΩ. Its bounce time is less than 1ms, and the LED’s current requirement is 20mA.

PTM Veröffentlicht am: