Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Same Mating Face

The internationally standardized connector family in IP20 and IP67 uses the same mating interface. This allows for the connector to be used as a service connector in IP67 devices. It also provides a great possibility of cost savings, as identical parts are being used for the mating interface. This shows the simple way of using single pair Ethernet in different applications.

PTM Veröffentlicht am: