Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
guide1
There are several basic guidelines that need to be considered when designing a vapor chamber into a thermal application. The first being that a vapor chamber thickness does not usually exceed 3 mm. Also, pedestals and other surface features can be used to contact specific heat sources while leaving clearance for other board mounted objects. These pedestals can be extended to 5 mm from the vapor chamber lid plate. Mounting holes can also be integrated within the area of the vapor chamber for better integration with the heat source and locating the heat source at the center of the vapor chamber with a good pressure application.
PTM Veröffentlicht am: