Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
part 2
When considering the use of a vapor chamber in an application, it is important to consider the orientation with respect to gravity and overall heat load for the thermal system. In many applications, the decision to use a vapor chamber is frequently compared to a thermal solution using heat pipes. In this seminar, Wakefield Thermal will outline the basics of vapor chamber operation, construction, and key application qualities that will be used to compare vapor chambers, as well as a heat pipe design.
PTM Veröffentlicht am: