Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
compar
One of the most common questions Wakefield Thermal is asked is how does a vapor chamber compare to utilizing heat pipes. The chart here explains the differences. It is important to consider the orientation with respect to gravity and overall heat load for the thermal system. Vapor chambers are best used in horizontal orientations. The effects of gravity may vary depending on application and orientation, but one must consider lower performance if used above 15° out of horizontal.
PTM Veröffentlicht am: