Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
PX PS Conductive Polymer Capacitors Slide 7

Shown here is a comparison of the ESR change with temperature change between conductive polymer aluminum solid capacitors and aluminum electrolytic capacitors. Again, the red line represents the conductive polymer while the green line represents aluminum electrolytic capacitors. As temperature drops, the ESR of an aluminum electrolytic capacitor significantly rises. Meanwhile, the ESR of a conductive polymer aluminum solid capacitor remains remarkably stable at low or high temperatures.

PTM Veröffentlicht am: