Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
PX PS Conductive Polymer Capacitors Slide 4

Here is a comparison of the conductivity associated with several different electrolytes. Note that the key to achieve low ESR is the device’s conductivity. Conductive polymer aluminum capacitors are constructed of a conductive polymer which is based on electron ionic conduction and which has extremely high conductivity when compared to other materials. In addition, with the further improvement to the conductive polymer electrolyte, PX/PS types have a higher heat resistance than other capacitors.

PTM Veröffentlicht am: