Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
PX PS Conductive Polymer Capacitors Slide 15

This chart shows a comparison of the ripple voltage elimination ability in the temperature range of 25°C to -20°C. Conductive polymer capacitors showed no change in ripple elimination ability at low temperature. The aluminum electrolytic capacitor’s ripple value tripled at -20°C. This phenomena is dependent on the capacitors’ impedance characteristics. The big difference in the test results is because aluminum electrolytic capacitor’s impedance increases at low temperature, and conductive polymer capacitors have nearly no change in impedance. Conductive polymer capacitors are clearly the best solution for applications used in environments with a wide range of temperatures.

PTM Veröffentlicht am: