Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 41

Moving on to even more highly integrated devices and offerings from Texas Instruments, there are devices dedicated to OMAP processors inside our TPS65 family. As can be seen, the OMAP processor brings many, many features with it, but also requires a larger power management solution. The TPS65 devices deliver the dedicated power management that the OMAP devices require. One of the features to consider is on the bottom right, the I²C interface which can help you reduce the amount of energy which you draw from the battery. For example, when the processor is running at high performance and it is driving multiple applications. This uses a large amount of energy coming from the battery. Even if not all the applications are running the processor is still requiring energy. With this usage, leakage and etc., it is drawing more energy from the battery than really needed. There are many types of losses which can be avoided. A way to do this is feed a signal from the processor back to the power management, the TPS65 devices can then regulate the voltage down and reduce overall power consumption to save energy needed from the battery. The drawback of a highly integrated power management unit is that power management is just at one spot. If it is necessary to distribute the power management, there is a risk of EMI due to transmitting the power across the PCB. In this case, it may be better for the additional application to have a single output linear regulator or DC/DC regulator.

PTM Veröffentlicht am: