Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 13

Shown on this slide are the key concerns for the analog front end, INA. On the left is a list of the more important features such as input bias current, input impedance, input current noise, voltage noise, power consumption, and DC/AC CMRR. Shown in the box on the right are less important features. This does not mean unimportant, only less important because they are offset related phenomena in the instrumentation amp. One thing to note is that the electrodes are going to have their own offsets which are going to change. Often times the DC errors that are introduced by the electrodes are going to swamp out the offset related errors that are inherent to the amplifier itself.

PTM Veröffentlicht am: