Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 4

A fully interactive diagnostic and patient monitoring block diagram which allows the user to review each segment of the analog signal chain, the MCU section, and the power management portion is available at ti.com. As an example, if the user selects the Input Buffer section they are able to choose, based on the requirements of an ECG system, a conditioning amplifier with the amount of precision or accuracy that is needed, the amount of SNR required, etc. The same can be done by selecting the ADC portion to determine whether a higher resolution or a lower resolution converter is needed.

PTM Veröffentlicht am: