Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Reed Sensors vs Hall and Electromechanical Slide 21

Reed sensors, in their hermetically sealed capsules, can switch as low as zero volts on up to 1000 volts with the same sensor and no added circuitry. Hall sensors in a magnetic field put out a low milli-voltage signal depending upon the strength of the magnet field. To switch higher voltages the signals need to be amplified and then sent to a power semiconductor. Electromechanical sensors cannot switch very low voltages or currents because they build up films on the contacts with usage. Usually five or more volts are needed to break over this film. They can directly switch up to 240 volts.

PTM Veröffentlicht am: