Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Reed Sensors vs Hall and Electromechanical Slide 19

Reed sensors have a low stable ON resistance, typically only 50 to 100 milli-ohms. Hall sensors have the resistance of semiconductor material and generally runs in the 1000s of ohms. Electromechanical sensors have a low ON resistance, typically in the 50 to 100 milli-ohm range. However, they generally will pick up a film on the contacts with usage, and unless its burned off by switching a relatively high voltage and or current, its ON resistance will increase. It could be at the 1000s of ohms level across the contacts. If users are only switching low voltages or low signals, they may be lost going through the high contact ON resistance.

PTM Veröffentlicht am: