Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Reed Sensors vs Hall and Electromechanical Slide 18

Hysteresis for reed sensors can be selected. This is particularly important if one is measuring the level of a fluid in a moving vehicle. A hysteresis of around 50% would be ideal. Here, once a low level, say of brake fluid is detected, the reed sensor will activate a light a light on the dashboard. With a 50% differential the light will remain on and steady. If the hysteresis was in the 90% range, the dashboard light would be constantly going on and off as the brake fluid slashed around with each bump or curve in the road. Hall sensors have no hysteresis. They have a gradual ‘ON’ signal and a gradual ‘OFF’ signal. Electromechanical sensors have a fixed hysteresis that cannot be controlled.

PTM Veröffentlicht am: