Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 36

In conclusion, the best time to use a linear regulator is when noise in the system cannot be tolerated or when the VIN and VOUT difference is small. The best time to use a switching regulator is when the difference between VIN and VOUT is large. Also, it is best to use a switching regulator when efficiency is important and large currents are involved. Semtech has many options for both linear regulators and switching regulators.

PTM Veröffentlicht am: