Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 21
In a voltage mode controller, VOUT is fed to the error amp through a feedback network. The feedback voltage is compared to a reference voltage. The difference between the reference voltage and the feedback voltage creates an error voltage. The error voltage is then compared against a sawtooth waveform by the PWM comparator. The output of the comparator then goes to the high-side FET driver to form the tON time. The two different waveforms of duty cycle show how different error voltages control the duty cycle. It can be seen that the total cycle time does not change, but the tON time and the tOFF time change to adjust the output voltage.
PTM Veröffentlicht am: