Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Power Supplies 101 Slide 14

This slide shows the basic waveforms associated with a buck regulator. DH is the control signal to the high-side FET. As the controller turns on the high-side FET, current ramps up in the switch. At the same time, current also ramps up in the inductor and the voltage of the phase node hits VIN. When the high-side switch is turned off, current ramps down in both the inductor and the low-side FET and the voltage at the phase node is pulled to ground. The signal at VPHASE is then filtered to form VOUT. The amount of time the high-side FET is on is defined as tON. The amount of time the high-side FET is off is defined as tOFF. The time of tON plus tOFF is defined as T, or total cycle time.

PTM Veröffentlicht am: