Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
come from ex2 hz
The engineer will use a Fast Fourier Transform (FFT) analysis that sweeps across all frequencies of sound for this fan against the sound pressure. One can see that big spikes occur for sound pressure at 280 Hz, 560 Hz, 840 Hz, and 960 Hz. Converting the fan speed from RPM to Hertz once again helps the engineer reveal the reasons behind these spikes in sound. 2,400 rpm is converted to 40 Hz, the 1st order frequency for this fan speed.
PTM Veröffentlicht am: