Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
opti inlet
Fans are sometimes installed onto the inlet side of the chassis, with the inflow of air through a perforated faceplate. This slide shows a variety of inlet obstruction examples that have been measured for sound pressure on a 9S0812M401 model. Shown here, the faceplate with the smallest perforations results in the highest sound pressure level, and this decreases with a combination of larger slit spacing and perforation pattern. The best sound pressure level comes from using a fingerguard, which allows for the most airflow into the fan. Obstructions on the inlet of a fan have a larger effect on sound than on the outlet side.
PTM Veröffentlicht am: