Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
come from ex1
Using the 9G fan model shown here with 9 blades per impeller and spinning at 11,000 rpm, the engineer can now calculate the frequency of wind noise. Start by converting the rotational speed of the fan from the RPM into Hertz, where 11,000 rpm equals 183 Hz. Multiply this by the 9 blades, and one can expect a peak from wind noise to occur at 1,647 Hz, as shown here in the bar chart of the recorded sound pressure per frequency band.
PTM Veröffentlicht am: