Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
DC-DC Converters in High Temperature Environments Slide 4
The I.C.E technology is a new technique of DC/DC converter construction that stands for Innovation in Converter Excellence. Developed by RECOM for its converters in the PowerlinePlus family. This new technology minimizes the internal power dissipation, maximizes the internal temperature limits and extends the ambient operating temperature range to the maximum. It improves the efficiency by 2 or 3% over standard designs (up to 92% efficiencies). This improvement may not seem to be substantial, but the power loss within the converter has been reduced by 20 percent.
PTM Veröffentlicht am: