Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
DC-DC Converters in High Temperature Environments Slide 10
As this presentation has shown, some of the struggles that engineers commonly face are in high temperature environments. With the new RECOM POWER DC/DC converters with ICE Technology engineers have the option of selecting a unique converter that includes all they need in one package: 100% of power without derating and high performance at a commercially acceptable cost. The main features of the Powerline Plus series from RECOM are its 2:1 and 4:1 input ranges, high isolation and protection, and a built-in FCC Class B Filter.
PTM Veröffentlicht am: