Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
CAS-Slide16

Due to the fluxgate principle, there is a significant ripple on the output with a fundamental frequency of 450kHz. The simplest way to attenuate the ripple is to add an RC low pass filter to the output. Drawbacks of the RC low-pass are reduced bandwidth if significant ripple attenuation is required, and degradation of dv/dt recovery time. Higher order filters or digital filters inserted after blanking can solve this.

PTM Veröffentlicht am: