Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
CAS-Slide10

The output of the transducer is centered around 2.5V with no primary current. With positive primary current, the output will rise to a maximum 4.625V. With negative primary current, the output will fall to 0.375V minimum. These values correspond to the peak measuring range of the transducer. For the positive and negative nominal currents, the output would be 3.125V or 1.875V respectively.

PTM Veröffentlicht am: