Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
CAS-Slide11

There are four accuracies listed on the datasheet. X includes sensitivity and linearity errors but does not include static offset while X at 85°C includes temperature-related drifts at the maximum operating temperature. XG also includes static offset. Also, depending on the application, it may be possible to calibrate out static offset.

PTM Veröffentlicht am: