Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Image of CUI Slide7

AMT absolute capacitive encoders consist of three basic parts as shown in the illustration above. The transmitter PCB emits an AC field that is distorted by the metal pattern on the rotor as it turns. A sinusoidal metal pattern on the rotor distorts the AC field in a way that is repeatable and predictable. This occurs as a result of varying capacitive reactance between the signal generated by the transmitter and the metal on the rotor. The field receiver uses the AMT ASIC to convert the modulated signal into digital position information, while the processor on the absolute encoder retrieves the position data from the ASIC and prepares it for export on the digital serial bus.

PTM Veröffentlicht am:
PTM Updated on: 2022-01-19