Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Image of CUI Slide10

Unlike quadrature encoders that repeat the same 4 states over a revolution, absolute encoders generate a unique digital ‘word’ for each position in its stated resolution. Because many absolute encoders are digital devices, resolution is expressed as an exponent of 2, otherwise known as binary. The numbers on the right of the absolute output illustration represent the numeric value of the bit when it is ‘on’ or ‘high’. A 6-bit (26) absolute encoder can generate 64 unique, digital ‘words’ that represent 64 positions over one revolution. Five positions are illustrated above. At the blue line, only the 20 bit is high, so the output is 1. At the green line, the 20, 21 and 22 bits are high: 1+2+4=7.

PTM Veröffentlicht am:
PTM Updated on: 2022-01-19