Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Image of CUI Slide14

SPI’s master-slave protocol and synchronous capabilities make it a viable option for many applications. The SPI protocol is fast and simple to use as most processors and controllers have SPI capability built-in. Its digital serial protocol also supports the inclusion of an error checking code into the position response allowing for greater assurance that the host received exactly what the slave sent.

PTM Veröffentlicht am:
PTM Updated on: 2022-01-19