Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Slide20
Finally, determine the ambient temperature of your circuit and then using the thermal derating chart on the data sheet, ensure that the PTC selected, has a higher Ihold value than the operating current, at this ambient temperature. When you have finished these 3 steps, you are well on the way to finding the ideal PTC for the application. Our course there are more details on our data sheets, such as time to trip charts, dimensions, resistance values, etc.
PTM Veröffentlicht am: