Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Slide15
As was mentioned earlier, Bourns is proud to have a range of the smallest size PTCs on the market. The PSMF series comes in an 0805 sized package and in a range of currents from 350 mA up to 1.1 A. Because of their size, these devices are amongst the fastest tripping PTCs on the market making them very useful in handheld and portable equipment. They can also be used in instrumentation, industrial, GPS and PC applications. 
PTM Veröffentlicht am: