Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide5
The Cyclone® III is the most aggressive family plan introduced from Intel®, with 8 devices in the family, 8 packages, 3 speed grades, 3 temperature grades, plus leaded and lead free packaging. With 30 density/package combinations, the family allows the maximum flexibility to choose exactly the right device and the ability to move between densities through vertical migration.
 
PTM Veröffentlicht am: