Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide25

A key area of focus for the Cyclone® III device family was optimizing memory to logic ratios for key high-volume, cost sensitive applications. Based on extensive customer design analysis and simulation, the on-chip blocks in Cyclone® III devices have been increased to 9kB including parity bits. The performance was also increased from 216MHz to 260MHz. Other features were added to increase flexibility and ease of use of the features. For example, Cyclone® III adds the ability to provide new data or old data when performing a read during write operation in Dual-Port mode. Quartus® II software can take advantage of the extra clock enables to reduce power by shutting off parts of the memory block when not in use.

PTM Veröffentlicht am: