Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
PDUs Slide 7

Networks are always growing. As additional hardware is added, eventually the input power source, whether it is a UPS system or a generator-supported wall outlet, will become overloaded. Once overloaded, circuit breakers will trip, causing network downtime. Metered PDUs provide a practical way for managers to enhance availability by preventing overload. Metered PDUs offer the same features as Basic PDUs, with the addition of a digital load meter. The meter allows network managers to locally view the total power consumption (in amps) of equipment connected to the PDU. As equipment is added, managers can see the increased load and take proactive steps to increase input capacity (with the addition of more or larger UPS systems or additional utility circuits). Tripp Lite offers Metered PDUs in low- and high-voltage versions to satisfy the power needs of all applications worldwide.  All models feature Single-Phase input.

PTM Veröffentlicht am: