Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
PDUs Slide 18

Most mission-critical network devices feature redundant power supplies (each with its own power cord) that can connect to separate power sources. Network managers need to guard against plugging the devices into a single PDU with a single power cord, which would eliminate failsafe redundancy. PDUs with two separate power circuits support the important fail-safe redundancy of devices with multiple power cords. Depending on the desired level of power protection, the two power sources can be two UPS systems, two generator-supported utility wall outlets or one UPS system and one generator-supported utility wall outlet.

PTM Veröffentlicht am: