Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Modular Test Leads Slide 2
TPI modular test leads allow for the selection of different ends or tips for a variety of applications. One modular lead can be used as a grabber, back probe, standard lead or as one of many other configurations because the lead ends and tips are easily interchangeable. As shown on the left side of the diagram, the first step in using the modular test leads is to select the lead type. Once the lead type is selected, then any lead tip from the right side of the diagram can be chosen depending on the requirements of the application.
PTM Veröffentlicht am: